Components Overview
Components are standardized, predefined graphics for defined use.
All drawn objects are either graphics, that is, free-form drawings, or components. A component contains one or several graphic figures. It can also have predefined functionality. Components typically represent a feature or a component in a live system. Components can be designed as symbols, which can be used as building blocks in graphics. Components are located in dedicated libraries and are displayed in the Components pane. An analog gauge is an example of a component.